5/8/2016 1:55 PM | |
Posts: 2 Rating: (0) |
Hello Everyone i am working on project on commissioning Phase ; the project is Master RTU controlling 2 RTUs , i am using CP341 as Master and 2 CP341 as Slaves with Modbus RTU protocol -Moxa Mgate is used to convert it into Modbus TCP and transmission is fiber optics , - Distance between MRTU and and 2 RTUs is 12000m and 27000 respectively it was working fully in FAT phase , now it is not attached assigned parameters for master and slaves , also diagnostic buffer for them. thanks for your Supports AttachmentMRTU screenshots.zip (38 Downloads) |
Follow us on