5/7/2016 12:48 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Which is servo motor? Which is drive? Which is software you are using to tune motor? |
5/8/2016 9:49 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... do you have problems in operation? Or why do you do the turning measurement at that high speed? The Motor has a ke = 148V/1000rpm ==> EMC = 666V at 4500 rpm. So your wide in fieldweakning. By the way, do you use a VPM (voltage protection module)? Maybe it is a problem of the current controller - high current is needed for fieldweaking (what stands in p320 ?) I would do a adaption of current controller (maybe to 30% at max. current Imax) But that´s all speculation. Following documents is important too: http://support.automation.siemens.com/WW/view/de/79690594 |
Last edited by: zako_ at: 5/8/2016 9:53:38 PM |
|
Follow us on