5/20/2016 9:03 PM | |
Posts: 1 Rating: (0) |
Hi everybody, I am configuring a Maintenance Station for my project and I need to select the Maintenance Station Standard but this option is disabled. I am working with PCS 7 V8.1 and I have already installed the Maintenance RT License as requiered. Can anybody help me with this. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/23/2016 12:36:08 PMNew subject after splitting |
|
5/23/2016 12:55 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hello Nataly, If you are sure you have the correct license, please check if you have sufficient PO objects. Also check the following: Select your project inside your multiproject->Right click-> PCS7 License information. You can see there what you are missing. If you added the license when Simatic Manager was open, please close everything, go to Simatic Automatic License Manager and right click the license and select: "Check". Now restart Simatic Manager. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on