5/25/2016 10:32 AM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (193) |
Hello Clemensen, my advice would be to use the rotation tool. It's an Excel Add-In that saves you a series of rotationg pictures with a discrete change of the angle between each picture. The background is transparent (.png). Connect the resulting graphics list to a symbolic I/O-field, assign a tag and it should work well. The rotation tool can be found here:
You can have a look at the chapter "Clarity" > "Gauge Controls for Basic Panels". They work in the same way I described above. Other Option: You can edit the look of the elements of a default WinCC Advanced/Comfort gauge. Just go to the properties and set every option where you can choose it to transparent, the fontsize to 1 and all dial elements in the layout section of the properties to 0 (besides the pointer hight of course). You will still be left with a triangular shape in a colour of your choice. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
5/25/2016 11:14 AM | |
Joined: 12/22/2014 Last visit: 9/9/2016 Posts: 4 Rating: (0) |
Thank you H.J.! I wasn't aware of this rotation tool, I will try it out this very moment! |
Follow us on