6/2/2016 4:59 PM | |
Posts: 7 Rating: (0) |
HI all I want to import Rosemount 3051ff to simatic pdm catalog ,i download dd file of 3051ff and when i try to import,i had this error: There is not any device to import.... can any one help me regards
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/3/2016 12:37:14 PMNew subject after splitting |
|
6/4/2016 3:09 AM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Mandegar; What version of the PDM device catalog are you using? It seems that Emerson (Rosemount instruments) sometimes does not provide a complete DD file in a format taht PDM can register. See the following FAQ: What should you do if devices which are imported subsequently are not displayed in the SIMATIC PDM device catalog (starting with PDM V6.0)? https://support.industry.siemens.com/cs/ww/en/view/22235967 SIMATIC PDM starting with V6.0, only supports the import of devices which correspond to a valid device class. This device class (e.g. sensor - flow rate - ultrasound) must be entered fully in the *.devices file from the device installation package. If there is a device class indicated which has not been specified by the PTO (PROFIBUS Trade Organization), this device is not transferred to the SIMATIC PDM device catalog. We did contact Emerson support fpr one such problem, and we did get some help. But the FAQ also proposes a solution that implies changing entries in the computer registers (regedit) that could help in some cases. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/4/2016 3:10:21 AM |
|
This contribution was helpful to1 thankful Users |
6/7/2016 2:50 PM | |
Posts: 7 Rating: (0) |
Hi Daniel Thanks Simatic PDM 8 Device Catalog 2-2015 |
6/10/2016 8:09 AM | |
Joined: 2/14/2012 Last visit: 4/25/2024 Posts: 31 Rating: (10) |
Hello Mandegar, I remember that the integration of the simple HCF or FF device description isn't possible. The DD must be created for SIMATIC PDM. I had a look to the PDM catalogue and in this some 3051 FF devices are integrated. Maybe you can try to import only the one necessary device from the catalogue. Here you can find the catalogue https://support.industry.siemens.com/cs/ww/en/view/109480121 Best regards, Patrik |
This contribution was helpful to1 thankful Users |
Follow us on