4/3/2008 1:21 PM | |
Posts: 279 Rating:
|
Hi Siwarexi. It is the Siwarex CF that I use, not the CS. Check out the note that follows each Siwarex CF module package (I have attached it to this post). It says that it cannot work with an IM151-7 CPU. You can setup a project in STEP7 with IM151-7 and Siwarex CF modules, and there are no error messages. But then why is the IM151-7 specifically mentioned in the note ? Attachment7MH4920-0AA01_pamflet.pdf (622 Downloads) |
4/3/2008 2:35 PM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Dear Mr. Pedersen, Sorry, I thought you mean the Siwarex CS module.Well, your product information is out of date.Attached you can find the current product information.There you can see, that you can use the Siwarex CF with a CPU which has a Firmware >= V2.1It is also expected, that the new PN-CPU will works with the Siwarex CF module. Best regards AttachmentProduktbeilage_CF.pdf (685 Downloads) |
4/3/2008 2:44 PM | |
Posts: 279 Rating:
|
Thanks for the information. That note I attached was picked out of a new Siwarex CF box one week ago. |
Follow us on