6/16/2016 3:35 PM | |
Joined: 12/4/2009 Last visit: 4/25/2024 Posts: 452 Rating: (134) |
dfgs, it's not possible to create complex tag types in WinCC V7.x. You can, however, talk to PLC via raw data tag - in that case you'll have to configure both PLC and WinCC side. As a result you'll get raw data tag which can be handled as an array of bytes(words, dwords, reals...). Members of this array can be accessed via C-script for example. There is more info on the following link: Exchange of large Data Volumes between S7-300/400 and WinCC with BSEND/BRCV Hope this helps. |
Last edited by: crazyCow at: 6/16/2016 3:36:29 PMLast edited by: The Helping Hand at: 6/16/2016 3:48:43 PMReplaced the link by a static one If this post actually helped, you may consider using the Rate button above. |
|
This contribution was helpful to1 thankful Users |
6/16/2016 5:25 PM | |
Posts: 10 Rating: (0) |
Thanks for the information XD |
Follow us on