6/15/2016 2:51 PM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33879 Rating: (4214)
|
Yes that is possible. Communication is via network inputs and outputs. Or about VM addresses. |
6/15/2016 3:16 PM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33879 Rating: (4214)
|
Here is a very simple network project as an example of communication between 3 Logo 0BA8.
AttachmentCommunication_with_3_0BA8.zip (230 Downloads) |
This contribution was helpful to1 thankful Users |
6/17/2016 1:08 PM | |
Joined: 1/30/2006 Last visit: 9/16/2024 Posts: 310 Rating: (58) |
Here is a short description and some screenshots showing how to set up the communication
AttachmentLogo V8 Communication Simple.zip (213 Downloads) |
BR. Sven |
|
Follow us on