6/25/2016 1:04 PM | |
Joined: 2/3/2014 Last visit: 6/30/2023 Posts: 1 Rating: (0) |
I have a similar issue, im using a 5.5Kw induction motor with a G120C inverter connected via PN on a 1215 PLC, i can get the motor to move on the drive commissioning but not on the axis commissioning and if i do it overshoots the position for ages then gives me a positioning fault! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/27/2016 3:27:27 PMNew subject after splitting |
|
Follow us on