7/1/2016 8:26 AM | |
Posts: 4 Rating: (0) |
Hello! I'm trying to configure a project with Comfort Panel using this manual with PCS7 Industry Library. I made all setup according that document and can't uderstand how it should work. For example, I have analog value monitoring block MonAnDi and panel block PMonAnDi. When alarm or warning appears, at the OS I can see messages of PMonAnDi block, so message view of faceplate MonAnDi is empty. And I can't see any message at the Comfort panel. What is the purpose of the PMonAnDi messages, if I can't see it at the panel? According the document, it's necessary to use Alarm_DQ (and use additional AS PO for it?). And document doesn't provide information how to use Alarm_DQ with main block (MonAnDi) and panel block (PMonAnDi). How can I setup blocks and messages to appear and acknowledge it from both the OS and the operator panel? Thanks in advance! |
7/4/2016 1:41 PM | |
Joined: 6/14/2006 Last visit: 6/17/2024 Posts: 301 Rating: (60) |
Yeah, that is what I understood. Anybody else with more information out there? Regards |
Follow us on