7/8/2016 10:18 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating:
|
Hi mvisconte, You can delete the tag logging archives in your WinCC project folder located under the OS project: "wincproj\<OSproject>\ArchiveManager\TagLoggingFast" and "wincproj\<OSproject>\ArchiveManager\TagLoggingSlow" - Open Taglogging - Select "Archives", right click->Archive configuration->TagLogging Fast or TagLogging Slow->Reset |
If I could help you, you can use the RATE button. Thank you. |
|
7/8/2016 10:35 AM | |
Posts: 72 Rating:
|
Thank you for your answer. I guess I could delete the files online in a C-Script, but that won't work, will it? |
7/8/2016 11:51 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating:
|
Hmm, maybe you can execute a .BAT file to delete the files. Maybe another (better) option, which Siemens does also is to make an image of the system and just put back the image after you are done. Then you always have a correct installation. Should take you 10 minutes generally. PS: Officially you have to remove your license keys before creating an image of a PC station. |
Last edited by: Oreca at: 7/8/2016 12:39:51 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on