8/22/2014 3:52 PM | |
Joined: 4/8/2009 Last visit: 7/11/2024 Posts: 35 Rating:
|
Hi everybody,
May be 6 out of 10 change only downloads to the OS server pair from the ES fails due to an error which says access is denied to the “..\ScriptLibStd:” The first download to the standby OS completes successful but in the second step to the master OS Server interrupts with the error. Which cause me to do an entire download to both of the server, which is not very nice you can imagine while the plant is running. It does not affect the operation that much but sometimes it causes to data loss as tag logging is stopped for a while. The reason I believe is that we have some cyclic running scripts on the os server and if the download happens while wincc is accessing the file. But is this normal? I’ve attached screenshots and log files for additional info. Any help is appreciated. Thanks Cem AttachmentOS1Srv UpdateErrorLog.zip (149 Downloads) |
Follow us on