7/18/2016 12:43 PM | |
Posts: 25 Rating: (0) |
How often i need to change battery in the old S7 300? |
7/18/2016 12:44 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Normally once a year (me) and never had problem Please have a look: When should you replace the back-up battery on your S7 300/400 ... |
7/18/2016 12:49 PM | |
Posts: 25 Rating: (0) |
And when the red led BATF light up, how long I have to change it? |
7/18/2016 12:52 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, as soon as possible, until you turn off the CPU. |
This contribution was helpful to1 thankful Users |
7/19/2016 11:29 AM | |
Joined: 7/9/2015 Last visit: 5/17/2024 Posts: 3833 Rating: (557) |
Hi Carfo, I think this FAQ will be also interesting for you: How great is the power requirement (from the backup battery) of the modules to be backed up at "Power Off" and what is the relationship between the backup current and the length of the backup time?This entry contains a small ZIP File "calculator.zip". With this file you can calculate the time... Regards, Towome |
|
|
This contribution was helpful to2 thankful Users |
Follow us on