7/17/2016 12:32 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, When reading your post, one thing that came up my mind is to use an Intlock block in APL library. The Intlock block (2,4 or 16 inputs) has the "FirstIn" parameter. It will show which signal was the first active. Maybe you can create your function with this standard PCS7 APL block?. You can use the "Reset" command to reset this "First signal" status. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on