7/21/2016 3:06 PM | |
Posts: 7 Rating: (0) |
Hello, I am a newbie to TIA SCADA. I have refered to Old topics and 'Help' documentation but couldn't find solution to the problem Problem: Version: TIA V13 SP1 Update 9 Hardware: 1 PC System with WinCC RT Professional and Industrial Ethernet, 2 Client PCs, Device Proxy Description: In the hardware configuration, I have used 4 device proxies to initialize data from 4 different machine PLCs. I am using one PC sytem with WinCC Prof connected with two client PCs. All are connected with 'Network-Industrial Ethernet'. When I started 'HMI Device Wizard', Which PLC proxy should I select to connect to WinCC RT Prof ? Since everything is connected in the network, Am I free to choose any PLC_Proxy initialized ? The attached screenshots give a clear picture Please help Thanks AttachmentScreenshots.pdf (177 Downloads) |
Last edited by: AutoGen_5650240 at: 7/21/2016 3:10:44 PM |
|
7/21/2016 3:51 PM | |
Posts: 7 Rating: (0) |
Thank you |
Follow us on