5/22/2009 6:59 PM | |
Posts: 28 Rating: (1) |
Sorry, I need to do this in Step 7 |
5/25/2009 9:23 AM | |
Posts: 28 Rating: (1) |
Thanks to all. I didn't know SCL, I must try this. I do the program in AWL so I put here the code AttachmentOrder Numbers.zip (165 Downloads) |
7/29/2016 4:25 PM | |
Posts: 4 Rating: (0) |
HI Guys, Here, I face with the same problems, in first step I`d like to sort five integers, that showing the operational hours of 5 pumps.I complete this section buy using bubble sort. what I want to do for my next step is to determine that which pump has Min operational hour and which pump is located in the second order, and so on. To achieve this i made an UDT, that included for different part, that listed below : Number : showing the pump number after selection, Before_Sort_Number : showing the pump number before selection, Operational_Time_NotSorted :showing the pump Operational hours before sorting, Operational_Time_Sorted : showing the pump Operational hours before sorting. Now the problems is that, the numbers sorted well but i cannot determine the the forth and fifth " Before_Sort_Number " correct. The code is attached, so I will be thank full to help me understand the problem. Regards Soroosh Shalileh AttachmentSorrtingPro.zip (133 Downloads) |
Last edited by: Sorooshi12 at: 7/29/2016 8:30:12 PM |
|
Follow us on