8/25/2016 6:53 AM | |
Joined: 4/7/2016 Last visit: 9/25/2024 Posts: 7 Rating: (0) |
Dear all I'm using 2 wire Analog input module for 4-20mA measurement for same I'm using Temperature Transmitter having output 4-20mA as well. but when I connect temp. transmitter wires to AI module, the counts overflows to 32768 & when I remove the wires counts goes to -32768 this is OK. but what about overflow value.!! I have used wiring scheme as per attached manual but still I'm getting this problem. any suggestions pls!! Attachmentet200s_2_ai_i_2_wire_st_manual_en-US.pdf (150 Downloads) |
8/25/2016 7:28 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Please give the model of temp transmitter. BR hristo |
8/25/2016 7:38 AM | |
Joined: 4/7/2016 Last visit: 9/25/2024 Posts: 7 Rating: (0) |
make is Endress Hauser model is TMR31 order no is TMR31-A1CAACAC1AAA |
8/25/2016 8:10 AM | |
Joined: 4/7/2016 Last visit: 9/25/2024 Posts: 7 Rating: (0) |
HOW TO TEST IT WITH MULTIMETER....?? |
8/25/2016 9:01 AM | |
Joined: 4/7/2016 Last visit: 9/25/2024 Posts: 7 Rating: (0) |
YOU MEAN, I NEED 4 WIRE ANALOG INPUT MODULE ? |
Follow us on