4/27/2016 9:01 AM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Hello dear COMOS Admins and users, it could be that you need to do the revision for some documents in COMOS. In such cases, you do not need to buy a PDF printer, as you can use the one which comes along with COMOS, which is called HARP printer.
- Please download at very first the full version of COMOS 10.1 from GTAC. - Download GhostScript 9.5, for 64 bits system, if you have a 64 bits system running - Run the delivered batch file, with the HARP printer, which comes with COMOS - Install GhostScript 9.5 - Choose the “Freely configurable revision printer” in the properties of the project, in COMOS itself - Revision your Report in COMOS, that’s it.
If you need/prefer to have a look into the official COMOS documentation for COMOS, please get the latest one here. They even have a German version there. At best, please use the search function in it, to get to the right pages about HARP.
Thanks in advance for your passion for such a great product as COMOS, with best wishes, SuperPippo AttachmentHow to install a HARP printer for COMOS 10.1.pdf (964 Downloads) |
Last edited by: SuperPippo at: 4/27/2016 11:49:04 AMLast edited by: SuperPippo at: 4/27/2016 12:17:24 PMLast edited by: SuperPippo at: 4/28/2016 10:31:00 AM |
|
This contribution was helpful to
1 thankful Users |
4/29/2016 9:34 AM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Hello everybody, if you prefer to see the homepage for the COMOS Documentation, from there decide if and which Documentation to download, here you have the link. All the best, SuperPippo |
4/30/2016 2:34 PM |
|
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating:
|
Thank you, Very useful.... |
7/13/2016 12:57 PM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Dear Dinesh, nice to hear from you. Please try the HARP printer from the COMOS 10.2 full version, as there was some issues with the mentioned operating system which they have solved there. If that does not helps, I'd suggest to open a new ticket at the Support of COMOS, adding as many information as possible, even the file which you have promised here. As soon there is a solution, we can than post it here, to share it with all the other users, if you like, if you agree. As well, please mention/document in that ticket (www.siemens.com/gtac) which steps you have done, which versions you have used, which error you see; if you prefer, you can attach to that ticket a video, which shows the whole information, steps and issue. A log file (recorded with the DebugView from Microsoft) would also be much appreciated by the people which will take care of it. All the very best SuperPippo |
Follow us on