8/23/2016 4:56 PM | |
Posts: 5225 Rating: (1185)
|
Which PLC exactly?.... |
8/24/2016 8:56 AM | |
Joined: 7/9/2015 Last visit: 4/26/2024 Posts: 3814 Rating: (554) |
Hello, I have got 2 examples for you as Link - for S7-1200/1500 and for S7-300 PLC. Check this: How do you read out the serial numbers of the SIMATIC Memory Card with the user program?How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
8/30/2016 5:08 PM | |
Joined: 7/21/2013 Last visit: 4/22/2024 Posts: 48 Rating: (0) |
How can I do ì my PLC has no external memory card Thanks Regards |
8/30/2016 5:14 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, the Get_IM_DATA only available for S7-1200 V4.1 or higher FW Version. For S7-1200 V2.2 this block can't be used. You should try the solution from this topic: (RDREC instructions) https://support.industry.siemens.com/tf/ww/en/posts/79804/
Christoph |
Last edited by: ChristophD at: 8/30/2016 5:16:02 PMLast edited by: ChristophD at: 8/30/2016 5:16:52 PMLast edited by: ChristophD at: 8/30/2016 5:17:07 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on