Industry Online Support
Technical Forum
3/11/2008 10:26 AM | |
Posts: 5822 Rating: (411) |
Hello Carles, maybe this FAQ may help you to solve this situation. Especially the first part may help you. Reconfiguring a DP slave via the Layer 2 access of CP5431 Best regards J_Bell |
3/13/2008 8:46 AM | |
Posts: 9 Rating: (0) |
Thank you very much. I'm going to take a look. |
4/18/2008 8:43 AM | |
Posts: 9 Rating: (0) |
Sorry, bu finally I didn't solve it. I was so close, but the client decided to connect with an S7. I think that the way is to create your net under COM Profibus and then create the GSD file. Then, you can edit this file andfind all the parameters that you need insideit (ID Vendor, User parameters). After that, you must setup the CP5431 with these parameters and modify the sample program that comes with this link that J_Bell passed us, with your data: Reconfiguring a DP slave via the Layer 2 access of CP5431 You can use the DP i/o test that comes with COM5431 to see if you get responses. I know that it's so tricky, so have luck !!! |
Follow us on