8/31/2016 1:49 PM | |
Joined: 5/6/2010 Last visit: 9/2/2024 Posts: 1978 Rating: (275) |
Hello, please look at the attachment, there is a manual. You connect this signal conditioner between your PLC and the proportional valve. You can configure your output signal if the input signal is lower than x.x mA (e.g. IN <4 mA then OUT = 4 mA). This is eplained in the manual. If you have more questions, let me know (part list etc.) regards Attachment106019_en_02.pdf (204 Downloads) |
Follow us on