8/24/2016 2:21 PM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello, with WinCC V7.4 WebNavigator license and WebUx is the same license they where called WebLicense. If the WinCC/WebUX option is also used in the WinCC system, a WebUX client can also occupya WebNavigator license. This reduces the number of available WebNavigator licenses. Fore more information you should read the following document 109736233 . If you have more question please ask. |
8/24/2016 3:06 PM | |
Joined: 1/15/2016 Last visit: 8/7/2023 Posts: 178 Rating: (4) |
Thank you for your answer. I am using WinCC V7.3. In this version, WebNavigator license and WebUX license are the same too? Thanks. |
9/5/2016 6:43 PM | |
Joined: 1/15/2016 Last visit: 8/7/2023 Posts: 178 Rating: (4) |
Thank you. Your answers helped me a lot. |
Follow us on