9/3/2016 9:17 PM | |
Joined: 11/5/2012 Last visit: 4/2/2024 Posts: 487 Rating: (63) |
Hello experts. Yesterday I had an issue uploading the software from a S7 1200 CPU. I tried with TIA V13, TIA V12 and TIA V11 but couldn't upload the software. I attach images of the errors. I read some FAQS about how to Upload the software, followed the steps but didn't work. :( Created an indentical station and then try to upload software but, errors were present. Used an unspecified 1200 to detect the configuration but I was only able to upload the hardware, not the software. I hope you can help me. Regards. Edited, underlined text. Attachmentupload errors.zip (269 Downloads) |
Last edited by: Rescobedo at: 9/4/2016 9:38:41 PM |
|
9/4/2016 2:37 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
According to this CPU's datasheet you need version 10.5 or higher. At this juncture it would be worth updating your version 10 to 10.5 and try it out and if it doesn't work I would go to version 11. BUT going by memory I think Simatic Automation Tool enables you to find project and hardware version information from the CPU. If that is accurate then it may be easier way to find exact information about the program version. |
This contribution was helpful to1 thankful Users |
9/4/2016 9:42 PM | |
Joined: 11/5/2012 Last visit: 4/2/2024 Posts: 487 Rating: (63) |
Hello. Firmware is 3.0. So, V12 and 13 won't work? I need to use V11? Regards. and thanks. |
Follow us on