9/9/2016 3:00 PM | |
Joined: 9/27/2006 Last visit: 6/29/2024 Posts: 12264 Rating:
|
Hello breno; There are some quirks to using As-i Safe, such as addressing the AS-i I/O modules (both standard and safe) with the CM As-i Master and activating the safety addresses through the F-CM As-i safety module. Note that some Safety I/O modules require 2 addresses, one standard, one Safe. Have you seen the following application note? It is very instructive: How do you operate an AS-i field bus system for different AS-i slaves with the CM AS-i Master and F-CM AS-i Safety modules? https://support.industry.siemens.com/cs/fr/en/view/109480137 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/9/2016 3:01:58 PM |
|
This contribution was helpful to
1 thankful Users |
9/19/2016 4:03 PM | |
Posts: 3 Rating:
|
Thanks Daniel, That was very helpful and got me well underway. Just have to wait to get the hardware in now. regards, Breno Romanini |
Follow us on