9/19/2016 9:53 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello dwb; WinCCViewerRT is installed along with WebNavigatoir client. This means you need a WebNavigator client installation on your PC (no license required), but you must first setup a licensed WebNavigator server, either on the same PC or in a remote machine. Here is an extract from the WebNavigator System manual: WinCCViewerRT The web viewer "WinCCViewerRT" is installed upon installation of the WebNavigator client. Procedure 1. Entry and check of the settings of the client computer in Internet Explorer. 2. Installation of the WebNavigator client. You can install the WebNavigator client as follows: ● Installation from the WinCC product DVD. In this case, certain Windows user rights are necessary, epending on the operating system. ● Installation via the Intranet/Internet. In this case, certain Windows user rights are necessary, depending on he operating system. ● Installation without user interaction: – Using the Windows user rights of the current user – Or in networks, using group policy-based software distribution In addition, you can also install the WebNavigator client on the WebNavigator server. This is useful, for example, if you want to check the WinCC project locally on the server in Internet Explorer. WinCC v7.3 WebNavigator - System Manual https://support.industry.siemens.com/cs/fr/en/view/102768445 Hope this helps, Daniel Chartier |
9/20/2016 9:36 AM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello, I think the following document help you to configure the Webnavigator 28309119. In this document they use Thin Client as Client to show the server pictures and informations. But in the Installation of the WebNavigator you can see the Client fpr WinCCViewerRT. Or alternative you can also use the internet explorer to show server pictures and informations. |
9/21/2016 1:09 PM | |
Joined: 1/15/2016 Last visit: 8/7/2023 Posts: 178 Rating: (4) |
Thank you all for the answers. |
Follow us on