9/19/2016 4:18 PM | |
Posts: 567 Rating: (106) |
Hi EJG, I would say that the number are only for one project or s7-program. You will find more information in the manual "PCS7 V6.1 PC Configuration and Authorization" chapter 3.6.4 |
This contribution was helpful to1 thankful Users |
9/20/2016 7:38 AM | |
Joined: 3/14/2008 Last visit: 5/6/2024 Posts: 2066 Rating: (928)
|
Hi EJG, Before PCS7 v7.x, the licenses were count like this: ES: PO levels: 250, 1000, 2000, 3000, 5000, unlimited. Where PO means a configurable process object in CFC. OS: PO levels: 250, 2000, 3000, 5000, 8500. One process object can contain approx. 30 tags. So when you see 4591 PO, you will need a PO license of 5000 |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on