9/23/2016 6:06 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello vavco. Just try out following points meanwhile you get the new NCU card. Remove the present NCU card, keep it outside as it is for 1/2 an hr. Remove & refit again, the battery from the card. This action will erase all data from the card. Clean the card carefully. Reinsert the card in NCU box. Switch ON power, (before switch ON power turn S3 ----> 1 & S4 ------> 2). Check the 7 segment display status. If it is OK , i.e. displays 6 & no any RED LED glows, try to reload the back up. CF - RED LED is COM-Watchdog has activated indication. (It is the problem in your case) CB - Data transfer via BTSS CP - Data transfer via MPI. Best luck. |
9/24/2016 6:41 AM | |
Joined: 10/17/2007 Last visit: 10/17/2024 Posts: 4047 Rating: (355) |
PISCEAN, I disagree with you this time. they should do like this-- No worry about NCU, new or old, No worry about NC card--PCMCIA card with NC sw. just insert PCMCIA card (old one They said is good) into new NCU any time they want, put NCU into NCU box. set S3-->1, set S4-->3. power NCU up. waiting until 7 segment LEDs display to "6" and left side LED only +5V green on (new version POK) this time PF will be on and PS will slowly flashing, ,set S4 from "3" to "2" and keep in "2" until PS flashing quickly at last stay on then set S4 to 0--the green PR should be on -- then NCU 1st time booting is finish--then they can download back up data NC/PLC PS: Have you ever seen the new, I mean the brand NEW 840D NCU (power line) , in its original Siemens box, when you open the box, you will see S3-->1, S4-->3, that is Siemens factory setting position. I can 100% sure as I did more 5 times customer services to replace NCU or making NCU upgrade. @vavco, can you please take the picture when you open the new NCU packing box and did not touch any switches, I'd like to see from the front the position of S3,and S4
|
Last edited by: nulizhang at: 9/24/2016 6:45:36 AM@vavco Last edited by: nulizhang at: 9/26/2016 3:03:15 AMLast edited by: nulizhang at: 9/26/2016 3:04:37 AMpcmcia CARD SHOULD be good with software If you like my comments please |
|
Follow us on