9/28/2016 11:48 AM | |
Posts: 25 Rating: (0) |
Hi Sirs, - I powered off control system and powered On to initialize all program. However it was still failed. AND after that, I select OB1, FC260, DB260 and download online to CPU again, then it is OK, FC27 worked well. In theory, when i powered on control system, CPU will be cold start and take the program in MMC loading to ROM then all blocks will be called and executed. But it is not same like that, modified blocks were only executed when i download OB1, FC260, DB260 at same time. This is first time i met this issue and it is difficult to give the exact answer. I am focusing on reason of error in calling FC260 call a sub FC27. Thanks a lot for your help. AttachmentOB1 call FC260.zip (44 Downloads) |
9/29/2016 6:46 AM | |
Posts: 25 Rating: (0) |
Hi Sir, I please send you the compile all report for analysis. FB141 not exist. FC27 has been protected, i do not know that whether it is reason. Thanks a lot. AttachmentCompile all report.pdf (40 Downloads) |
Follow us on