8/30/2016 8:53 AM | |
Posts: 18 Rating: (0) |
I am configuring Scalance S612 in routing mode. I have refer the installation manual and configured the external and internal port accordingly. Software Used - Security Configuration Tool V04.01 External Port : 192.168.1.222 ----- IP address of Router Internal Port : 192.168.0.10 ----- IP address of PLC But when I transfer this configuration to module, it is showing error message as "The attempt to connect to IP address 192.168.0.10 has exceeded the time limit" and message pop up as Transfer failed. Attached herewith the snaps of configuration window and error message. Please help me to resolve this problem:( Attachmenterror snaps.zip (195 Downloads) |
9/29/2016 4:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by nkr is split to a separate thread with the subject Scalacne S612, Error while downloading configuration. Best regards |
Follow us on