10/1/2016 4:06 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: A new feature of STEP 7 V14 is the possibility mix LAD/FBD and SCL language in the same blocks Requirements: TIA V14 S7-1200 / S7-1500 / ET200SP CPU TIP: Each network contain just one type of language It is not possible to change the language of a network but it is possible to add a SCL network in a LAD/FBD block. Configuration main steps:
Cast: Due a size/ format restrictions, a cast of the SCL network insertion was archived as 7z format and after that as .zip format. Attachmentscl.zip (176 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
10/1/2016 4:40 PM | |
Posts: 5225 Rating: (1187)
|
To IBN-Service ... Was this not the feature you asked for? This feature I will like very much! |
Last edited by: William_B at: 10/1/2016 4:47:06 PM |
|
This contribution was helpful to3 thankful Users |
10/3/2016 11:18 PM | |
Joined: 3/30/2011 Last visit: 5/12/2024 Posts: 733 Rating: (255) |
<kidding> new feature for step7 tia........... But I was used to mix different language segment with step5.... Talking about "steps" there is an italian saying that goes: 'one step forwards and two steps backwards' </kidding> thank you to Denilson Pegaia for his valuable contribution |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
Follow us on