4/24/2008 5:53 AM | |
Joined: 9/27/2006 Last visit: 4/30/2024 Posts: 12257 Rating: (2666) |
Hello PC4; Here is one suggestion (there are other ways of doing this, of course). Draw your water tank as a static object; insert a "BAR" object (this is a scaled bargraph object) and link the Fill property to a tag that will change value dynamically to give you a numerical value of the fill level. If your PLC is calculating the level height from some kind of transducer, simply link thios to the BAR object properties. There is a detailed example on how to do this in the WinCC Flexible Getting Started manual; you will need to adaot it to your needs of course, but it explains the principles and the steps to do it. Hope this helps, Daniel Chartier |
4/24/2008 6:01 AM | |
Posts: 487 Rating: (36) |
Hi In 'TOOLS' under 'simple objects' use the 'BAR' Connect a tag of the integer type , sett a min max value .under animation , appearance you can select ranges and connect different colors to it .Have a look at the getting started manual Eric Oops , Daniel you replied a bit faster than me but its the same |
Last edited by: aikona at: 4/24/2008 6:04 AM |
|
Follow us on