10/9/2016 6:04 PM | |
Joined: 9/23/2005 Last visit: 9/11/2024 Posts: 4347 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: in this simple sample, one HMI screen is copied from the project library to the HMI project following the controller FB properties. Requirements: TIA V14 SiVArc Project with a minimum configuration: S7-1500 configuration, Configuration main steps:
Result: the “MyHMIScreen” is copied from the project library to HMI Screens folder References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap14 format and after that attached to a zip archive (.zip). Attachmentproject.zip (158 Downloads) |
Denilson Pegaia |
|
Follow us on