10/10/2016 3:42 PM | |
Joined: 3/14/2016 Last visit: 8/11/2023 Posts: 162 Rating: (45) |
Hi, what was the error value read? For measurements between 1-5V and 0-20 or 4-20mA, here are the possible values for analog modules: What is the configuration of the module? Go to the PLC Device Configuration and right click on the Module under Proprieties/Configuration. Maybe it can be filtering or settings. I'll attach the PDF for Analog Modules. AttachmentAnalog Module.pdf (105 Downloads) |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
Follow us on