10/17/2016 8:28 PM | |
Posts: 30 Rating: (0) |
|
10/17/2016 8:29 PM | |
Posts: 30 Rating: (0) |
AttachmentHAT1000_diagnostic-err.txt (53 Downloads) |
10/18/2016 8:36 AM | |
Posts: 30 Rating: (0) |
Hi DJ_1, Yes I checked the accessible device in TIA Portal and there is only CPU connect via profinet check attachment there is the picture. On the profibus card I can not read the device address of ET200s adr is 8 I do not see this device . In profibus network, the starting device Profibus connector terminating Register and End device Profibus Connectro Terminating Register are ON and middle device is OFF. I checked two times. I do not know where I check fw version of IM. Could you tell me how to do it? If I connect only Second Device (Encoder) it is OK and when I connect only ET200s I do not configure this device. I do not know why. Peter AttachmentProfibus-Err.zip (39 Downloads) |
10/18/2016 1:20 PM | |
Posts: 30 Rating: (0) |
Hello Christoph, Yes I can tell you more about the wiring. I have 3 connectors on bus 1st one is plug to CPU 1214C and switch is ON(A1-B1), 2nd is on IM 151-1 Basic and switch is OFF (A1-B1 & A2-B2)and last one is plug tu encoder and switch is ON (A1-B1). The midle is plugin to the IM 151-1 Basic. When is midle conector connected the booth devices (et200s & encoder) is not reachable. When I disconnected this midle conector the last one device is OK. I tried connect only IM 151-1 still not reacheble, one by one (two connector, switch are ON) Peter PS: I conected lihe here. EDIT: I catch error on IM 151-1 Basic |
Last edited by: PeTer111122 at: 10/18/2016 2:03:17 PMLast edited by: PeTer111122 at: 10/18/2016 2:03:30 PMLast edited by: PeTer111122 at: 10/18/2016 2:30:42 PM |
|
Follow us on