10/20/2016 7:50 PM | |
Posts: 3 Rating: (0) |
Good morning BeVee. I have the same problem.... but I am using Tia Portal RT Advanced V13 SP1: In STEP MANAGER: I have configurated the tag in the PLC's DB (DB5 type STRING[10] two byte header - Bytes from 0 to 12, 2 first bytes header) I can see into DB5 the characters of the string ('T2959A7216') in online mode. Thats OK In Tia Portal HMI: 1. I configurated the HMI Variable Name: Recipe Type: Array[0..9] of Char Conexion: that is configurated OK Address: %DB5.DBX2.0 (I skip two first bytes because is header info) 2. Field for display Display Format: String String field length: 10 Tag: Tag name The display in the HMI screen of the Recipe NAME is OK. My question: How can I Record in a ".csv FILE" this information of the string? because tia portal RT Advanced configuration does not accept save variable type string. Thank you for your help and support. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/21/2016 2:33:00 PMNew subject after splitting |
|
Follow us on