10/25/2016 10:05 AM | |
Joined: 7/6/2016 Last visit: 3/18/2021 Posts: 20 Rating: (1) |
Hello! Can you link me concrete product for these servos? Or what are the differces between S110 and S120 models? |
10/25/2016 10:18 AM | |
Joined: 5/12/2006 Last visit: 7/30/2024 Posts: 22330 Rating: (2999) |
Hello, S110 is a single drive system to control one Motor, you combine a Control unit with a power module and connect the motor to the Power Module, the communication between PLC and Motor is task of the Control unit. S120 is a multiple drive system, here you can control up to 6 Servo Drive from on Control unit. You need a Control unit, a infeed unit and one or more motor Modules. Links: https://mall.industry.siemens.com/mall/en/de/Catalog/Products/10122049?tree=CatalogTree https://mall.industry.siemens.com/mall/en/de/Catalog/Products/10045435?tree=CatalogTree Regards Christoph |
This contribution was helpful to1 thankful Users |
Follow us on