10/25/2016 4:32 PM | |
Joined: 3/14/2008 Last visit: 5/6/2024 Posts: 2066 Rating: (928)
|
Hi, On the client, open WinCC Explorer, right click on Server Data and select Standard Servers option. In the Standard Server dialog box select SSM (Split Screen Manager) and select your server. This is the basic configuration for a PCS7 client. When no standard server is assigned for SSM, trends get stored locally on the client. When a standard SSM Server is assigned, the trends are stored on the selected server. All clients with the same standard server will be able to see any trend created on any of these clients (and servers). |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on