10/27/2016 10:45 AM | |
Joined: 10/11/2016 Last visit: 12/7/2023 Posts: 3 Rating: (0) |
Hi, Has anyone seen problems with this where installing an update to TIA portal does not add the hardware? I have TIA Portal v13 update 9 and this does not include the ET200SP CPU (part number 6ES7512-1DK01-0AB0) in the catalog - see attached screenshot. I have checked that all HSP files are current and installed - they are - but still I do not see this CPU. Richard. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/28/2016 3:20:04 PMNew subject after splitting |
|
10/27/2016 10:51 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, for the Hardware you need to search for HW Updates. in the TIA updater you can search for Software and for Support Packages. Or download it here: Support Packages for the hardware catalog in the TIA Portal (HSP)
regards, |
FCK WAR! |
|
Follow us on