4/20/2008 11:15 AM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello Abdelaal; On the Installation CD of the Modular PID software, you should find a project "zEn28_04_ ModCon" Actually, the setup program should have made it available in Step 7 (under File, Open, Samples). That project is made up of 12 different examples of PID control using the Modlar PID blocks. The first 3 are basic closed-loop applications that should help you understand the different blocks and their interconnections. On the same CD there should be a manual PID_e.pdf that explains the examples and the blocks. It should have been added to the Simatic-->Documentation folder on the computer where you have installed the software.If you cannot find it look here: |
4/24/2008 2:32 PM | |
Posts: 76 Rating: (16) |
dear Böhser_Onkel , I think you are right , as i only have one cd not two. Thanks for your reply . It's all now clear regards |
4/28/2008 10:44 AM | |
Joined: 4/24/2008 Last visit: 8/2/2024 Posts: 213 Rating: (16) |
no problem |
|
|
Follow us on