11/11/2016 2:31 PM | |
Posts: 439 Rating:
|
Hello Kal.A, Ok let me explain then. There are the HMI panels, which are the Basic panels, the Key panels, the Comfort panels and the Mobile panels. It is also possible to install WinCC Runtime Advanced or WinCC Runtime Professional on a PC base, like an IPC (Industrial PC). I hope it clears everything. Best regards, Hugo |
11/11/2016 2:58 PM | |
Posts: 439 Rating:
|
Hello Kal.A, You are jumping from one question to an other one, which is hard to follow. Create a new post if you have question related to upload of a S7-1200. Your question will probably be split into a new post anyway. You asked about "Recipe queries", which is only available in WinCC Runtime Professional, see attach file. You can use recipes in basic, comfort and runtime, see the excel comparison table in the link below. What are the functional differences between the different SIMATIC panels?Best regards, Hugo AttachmentAdv vs Pro.zip (112 Downloads) |
Follow us on