11/15/2016 2:47 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Fritz wrote: 124 (not 125) DP Slaves is (should be) the maximum number of DP Slaves per DP Master interface of an S7. and another info from fritz: Max Address Settable in Profibus DP - Entries - Forum - Industry ... |
11/16/2016 9:45 AM | |
Joined: 9/29/2016 Last visit: 2/26/2024 Posts: 25 Rating: (3) |
Hello Thanks for replying. but my set PG/PC setting is showing address from 1 to 126. and 0 is address of PG/PC so total devices must be 126. 1 master and 125 slaves |
11/16/2016 11:12 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Dear aswin, please have a look in particular at page 16 : |
Last edited by: Ste39 at: 11/16/2016 11:17:52 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on