12/14/2016 6:32 PM | |
Posts: 1 Rating:
|
Hi ! I'm Hung, I live in Vietnam. I have read your answer in an article on High Speed counter flow. I'm having a little problem on High Speed Flow counter wish you help me? thank you! The problem I see is as follows: in Vietnam I used flow sensor S201 (link: http://banlinhkien.vn/goods-3136-cam-bien-luu-luong-s201.html) to measure water flow 1 discharge of water tanks. I use PLC S7-200 CPU 226 AC / DC / REL to count the pulse sensor, but I still have not written to the PLC Program Block. You can help me solve the problem there? I'm very urgent need to look forward to your reply to me. Thank you for reading this quote of mine. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/15/2016 10:14:36 AMNew subject after splitting Last edited by: Min_Moderator at: 12/15/2016 10:17:10 AMContact data deleted and add links Last edited by: Min_Moderator at: 12/21/2016 1:36:53 PMAdd one more link |
|
12/15/2016 12:04 PM | |
Posts: 5225 Rating:
|
Maybe have a look at the picture. The System Manual for the S7-200 is also full of information.
|
Follow us on