5/7/2014 8:39 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello cherlokx Sorry to disappoint you, but if the machine was powered off with Low Battery and no EPROM, then in all possibility the program in CPU RAM is Lost. It can only be re-loaded from the program stored in EPROM or from a Soft Copy Backup Hope you are able to get hold of one of these Cheers Navnag |
There is no such thing as the last bug in a program |
|
12/25/2016 9:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by norimane is split to a separate thread with the subject S5-100u cpu, message "$ 613 DB-Fehler Nr. 10 ( 0;10)". Best regards |
Follow us on