Industry Online Support
Technical Forum
12/17/2013 1:11 PM | |
Joined: 10/11/2007 Last visit: 3/14/2024 Posts: 2 Rating: (0) |
Hi everyone, I have a automation network with several PLCs communicating between them and Step7 server trough ethernet. Each PLC has an ET200M connected in Profibus DP to the CPU 313C-2DP and each ET200M has one or more flowmeter connected in HART. In the server I have installed the SIMATIC PDM v6.0 and in the hardware configuration I have selected the flowmeter in the hart field device. I can make the upload/download of the flowmeter settings to PDM I need to generate an verification certificate like the verificator certificate MAG 8000. Normaly, to get the verification certificate I need to go locally with the flowmeter and get the verification trough HART comms using the Pactware software. See in attachment one verification certificate... Its different from the calibration certificate (4-20mA). My problem is how to get an verification certificate with SIMATIC PDM v6.0. Anyone knows if its possible? Does version v8.0 generate this certificate? Do I need to install any add-on? In attachment there goes an Krohne verification certificate and an PACTWARE verification certificate. Thanks for you attention. Best regards. DSilva AttachmentVerification certificates.zip (69 Downloads) |
1/4/2017 10:40 AM | |
Posts: 1 Rating: (0) |
Ninguém te responde... LMachado |
Follow us on