1/2/2017 4:00 AM | |
Joined: 12/7/2011 Last visit: 8/16/2024 Posts: 384 Rating: (9) |
Hi guys, and happy new year to all Since two weeks ago, I've faced one problem with the PDM. The system involved was: PCS7 V8.0 sp1 and PDM V8.0 sp2. Ok, let's start, two weeks ago (more or less) I've installed the PDM in my EWS, once the installation was finished, I've load the necessary licences and reboot my EWS, but as you can image, the PDM doesn't start. From that moment I've tried all possible solution that you can image, reconfigure my Maintenance station, deinstall and reinstall again, recompile everythings (hw included),consistency check (hw included), and more and more. One day I decide to export the HW config, delete all (except the CPU's) and reimport again, and since that moment, i get a consistency error! . the first question is: How is possible that, no one error is apperared during the HW consistency check, and during the HW import yes? Pratically the error was referred to an ET200M Master assignement, it seems that when the ET200M it's been created, the DP Master it's been assigned as a Rack1 the first master, and Rack0 the second. In this condition I wasn't able to reimport the HW config anymore, so I've retrived the last backup, fix the problem in the HW config, export, reimport (without error) compile, and as for magic the PDM start to work. . From this experience, I have some questions to Siemens, that are: How is possible that, no one error is apperared during the HW consistency check, and during the HW import yes? Is it possible that a small error like that, prevent the PDM functionality? Thanks for all of you that will enjoy this Tip. Regards. Duccio. Attachmentpdm.pdf (105 Downloads) |
Last edited by: Duccio at: 1/2/2017 4:40:37 AM |
|
Follow us on