7/11/2014 3:44 PM | |
Posts: 1058 Rating: (93) |
I have forwarded your problem to Siemens development. If I get an answer I will tell you here. regards |
7/15/2014 8:43 PM | |
Posts: 4 Rating: (0) |
Has this been solved yet? I have the same issue. |
Last edited by: DylanPeterMiller at: 7/15/2014 8:45 PM |
|
7/16/2014 10:11 AM | |
Posts: 1058 Rating: (93) |
There are several users with same problems. That is why I forwarded it. But I have no reply yet. As soon as I get an answer I will post it here. regards |
7/17/2014 1:05 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating: (110) |
Hello CN Mark and DylanPeterMiller, I havn't got this problem up to now. But a friend told me that other programs in the background like scanner for viruses could be the reason. Please try to start the software Block Privacy first and than the other programms. This should avoid the behavior. Please keep us informed about your success Best regards Sabine |
7/17/2014 2:56 PM | |
Posts: 1058 Rating: (93) |
According to Siemens, this problems might arise because of active background programs (i.e. virus scanner etc.). Close down background programs and then start block privacy. Once block privacy is running, you can activate background programs again. Regards |
8/4/2014 11:03 AM | |
Joined: 11/15/2012 Last visit: 9/19/2024 Posts: 1 Rating: (0) |
Hello, I've same problem. I've try also deactivating antivirus, but Block privacy appears for only a short instant and then it shuts down. How other user have solved this problem ? Many Thanks |
1/10/2017 10:16 AM | |
Posts: 2 Rating: (0) |
Hi i had the same issue and tried to stop the background process one by one using the windows command services.msc, and to launch the Block Privacy utility. i'm using a pc with Windows 7 Professional, S7 v 5.5 +SP4. After stopping Office Software Protection Platform it runs normally |
Follow us on