9/16/2013 10:34 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User rgurjar
|
9/16/2013 1:51 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear Friend, Please check Ethernet cable too.... |
Last edited by: Amit_86 at: 9/16/2013 1:53 PMVANDE MATARAM..... |
|
9/17/2013 9:24 AM | |
Posts: 107 Rating: (1) |
If I gave an answer that would be probably the one place in the statistics of users. What is the point of giving so hopelessly delicious solution? The problem actually exists in combination Step7 v5.5 and Step 7 V12SP1. Neither the v5.5 or under V12SP1 not be editing tools on the network settings created for this purpose - Edit Ethernet Node - no matter where you start - Simatic Manager, HWCONFIG, NCM Diagnostics. So reason we do not have to smile too much. |
9/17/2013 10:26 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
IF YOU HAVE SO MUCH KNOWLEDGE COME HERE REGULARY AND ANSWER THE QUESTION |
VANDE MATARAM..... |
|
9/17/2013 10:31 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
ONE MORE THING I THINK YOUR EYE SIGHT IS WEAK. THE QUESTION PUBLISHED BT IMPORT USER FROM SOME x USER & HE HAS NOT MENTIONED THAT THERE ARE COUPLE OF SOFTWARE INSTALLED IN PC. HE HAS JUST MENTIONED STEP7 V5.5 NOW , DID THE USER CAME IN YOUR DREAM LAST NIGHT? |
Last edited by: Amit_86 at: 9/17/2013 10:44 AMVANDE MATARAM..... |
|
11/14/2013 9:52 AM | |
Joined: 4/29/2010 Last visit: 5/2/2024 Posts: 26 Rating: (0) |
Hey All, Please check your firewall settings. Using SEP, you have to disable the firewall. This solved it for me |
1/23/2017 12:00 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by Ashish279 is split to a separate thread with the subject Edit Ethernet Node not showing anything. Best regards |
Follow us on