1/18/2017 4:19 PM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Hello, When you have Step 7 v5.x, you should buy the optional package S7-Distributed Safety. Best regards, Wizard |
1/22/2017 5:52 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi strmin123, Profisafe is similar to Profibus but in addition, it has safety features like frame, signatures asd self tests. You should install following software in sequence- 1. For F-system- CFC, F-configuration pack and S& F systems and F-library. This is used for process applications. 2. For distributed safety- F-configuration pack and Distributed safety. This is used for machine or factory automation. Make sure that the version compatibility among these software. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
1/23/2017 5:03 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi strmin123, 1. Yes, Configuration pack is related to hardware configuration. It provides F-relevant parameterization available in HW confi. after installation. 2. You have to use either F-systems or distributed safety. For F systems, CFC is compulsory. For Dist. safety, u can use F-LAD or F-FBD. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
1/24/2017 3:53 PM | |
Posts: 8 Rating: (1) |
Thank you! It is very helpful information. But, It is so hard and complex.... I have to read more! Thank you. Have a nice day. |
Follow us on