2/17/2016 11:24 PM | |
Posts: 1 Rating:
|
Hi When I try to connect it, it immediately damaged, even though the wiring as per the datasheet here https://www.downloads.siemens.com/download-center/Download.aspx?pos=download&fct=getasset&id1=BTLV_43430 The building have L, N ,and Ground , 1 phase 220 V 50Hz I connect the black wire to the L The white wire to the N the green to the ground NOTE: The
device have tape with (120V) even though the device clearly indicate
that the voltage is 240/120V (attached) I doubt it is the problem but I
have to mention it. I'm going to buy/replace it but I need to know what I did wrong as every thing seems OK until it connected , Any suggestions? Regards Attachmentfs_100.zip (931 Downloads) |
4/25/2016 1:59 PM | |
Joined: 10/10/2010 Last visit: 4/28/2024 Posts: 307 Rating:
|
Higher voltage than rated can damage the surge protector completely |
1/29/2017 8:36 AM | |
Posts: 2 Rating:
|
thanks |
Follow us on