2/6/2017 1:02 PM | |
Posts: 13 Rating: (0) |
Dear Gents, How can i select the ACB e.g stands for what 3WL1216-4EG45-4GA2 |
2/7/2017 7:31 AM | |
Posts: 1 Rating: (0) |
It is ACB 4 Pole 1600 A frame size 2 draw out version without guide frame ETU45 LSING with Motor/closing220VAC with Shunt release 230 V AC / 220 V DC without under voltage , 2NO + 2NC (standard) auxiliary switches For More info , please visit Attachmentcoding ACB.pdf (218 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on